Solid Edge FrameworkSupport Type Library
AddSurfaceFinishSymbol Method
Description
Creates a SurfaceFinishSymbol. For creating PMI SurfaceFinishSymbol a plane must be set (XY plane is the default). The collection object from which it is derived (sheet/profile2d/PMI) dictate the creation of SurfaceFinishSymbol.
Syntax
Visual Basic
Public Function AddSurfaceFinishSymbol( _
   ByVal AnnotInitData As AnnotInitData _
) As SurfaceFinishSymbol
Parameters
AnnotInitData
See Also

SurfaceFinishSymbols Collection  | SurfaceFinishSymbols Members  | Solid Edge ST5 - What's New

Send comments on this topic.