Solid Edge FrameworkSupport Type Library
ClearDataSet Method
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
SurfaceFinishSymbols Collection
: ClearDataSet Method
Description
Restores the property settings applied to existing annotation objects.
Syntax
Visual Basic
Public Sub ClearDataSet()
Remarks
These settings remain until the DataSet property of the annotation collection object is modified.
See Also
SurfaceFinishSymbols Collection
|
SurfaceFinishSymbols Members
Send comments
on this topic.