Solid Edge FrameworkSupport Type Library
Index Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
SurfaceFinishSymbol Object
: Index Property
Description
Returns the numeric index for the active object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Index As Long
Remarks
This index is the sequence that the object holds in its collection object (as held by the parent).
See Also
SurfaceFinishSymbol Object
|
SurfaceFinishSymbol Members
Send comments
on this topic.