ActualTextLength | Returns the length of the character string in the longest line of text. |
Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
BorderLineColor | Sets and returns the color used to draw the border of the referenced TextBox object. |
BorderLineStyle | Sets and returns the line style used to draw the border line of the referenced TextBox object. |
BorderLineWidth | Sets and returns the color of the border when BorderVisible is True. |
BorderOffset | Sets and returns the distance between the border and the text box for the referenced TextBox object. |
BorderType | Sets and returns the border type for the referenced TextBox object. |
Document | Returns the document to which the referenced object belongs. |
Edit | Returns the TextEdit object associated with the referenced TextBox object. |
Fill | Specifies whether or not the background of the referenced TextBox is to be filled. |
FillColor | Sets and returns the color with which to fill the background of an object. |
FlowOrientation | Sets and returns the orientation of the text flow. |
Height | Returns the height of the referenced object. |
HorizontalAlignment | Sets and returns the horizontal alignment of the text within a paragraph. |
Index | Returns the numeric index for the active object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Justification | Sets and returns the horizontal and vertical justification of the text for the referenced TextBox object. |
Key | Returns a key (a string) to find the object relative to its owning parents. |
KeyPointCount | Returns the number of keypoints/handles that are supported by the referenced object. |
Layer | Sets and returns the named layer on which the referenced object resides. |
LineSpacing | Sets and returns the amount of space between two lines in a paragraph for the referenced object. |
LineSpacingType | Sets and returns the Line spacing type for the referenced TextBox object. |
MinimumAspectRatio | Sets and returns the Minimum Aspect Ratio Textbox can have |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
PlacementType | Sets and returns the placement type for the referenced TextBox object. |
RotationAngle | Sets and returns the angle, in radians, at which the object is rotated along its major axis. |
Shadow | Specifies the status of the shadow feature for the referenced TextBox object. |
ShadowOffset | Sets and returns the offset of the shadow feature from the border for the referenced TextBox object. |
TabStopWidth | Sets and returns the default Tab Stop width for the referenced TextBox object. |
Text | Sets and returns the text within the referenced TextBox object. |
TextControlType | Sets and returns the Text Control type for the referenced TextBox object. |
TextScale | Sets and returns the text scale of the object. |
Type | Specifies the type of the object being referenced. |
VerticalAlignment | Sets and returns the vertical alignment of the text within the text box. |
Width | Returns the width of the referenced object. |
ZOrder | Specifies the front-to-back order in which an object is displayed relative to other objects. |