Solid Edge FrameworkSupport Type Library
Scale Method
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
WeldSymbol Object
: Scale Method
Specifies the factor by which the referenced object is to be scaled.
Description
Scales the referenced object by a specified factor.
Syntax
Visual Basic
Public Sub Scale( _ ByVal
Factor
As Double _ )
Parameters
Factor
Specifies the factor by which the referenced object is to be scaled.
See Also
WeldSymbol Object
|
WeldSymbol Members
Send comments
on this topic.