Solid Edge Framework Type Library
Remove Method
Collapse All
Expand All
Solid Edge Framework Type Library
>
Accelerator Collection
: Remove Method
Specifies the key code of the KeyBinding object to be removed.
Description
Removes a specified object from the referenced collection.
Syntax
Visual Basic
Public Sub Remove( _ ByVal
KeyCode
As Long _ )
Parameters
KeyCode
Specifies the key code of the KeyBinding object to be removed.
Remarks
Remove removes the KeyBinding object that maps to the specified key code. The call succeeds even if no object identified by the input key code exists.
See Also
Accelerator Collection
|
Accelerator Members
Send comments
on this topic.