| Class Module | Description | 
|---|
| Accelerator | Represents a collection of KeyBinding objects. | 
| Accelerators | Represents a collection of Accelerator objects. | 
| AddIn | A control that represents a command added to Solid Edge through the AddIn interface. | 
| AddInEdgeBarEvents |  | 
| AddInEvents | A collection of AddInEvent objects. | 
| AddIns | A collection of AddIn objects. | 
| Application | Provides the properties and methods necessary for a Visual Basic user to drive Solid Edge programmatically. | 
| ApplicationEvents | Fires application events. | 
| ApplicationV8DocumentOpenEvent | Fires document open event | 
| ApplicationWindowEvents | Provides access to the application window events. | 
| AssemblyFamilyEvents |  | 
| AssemblyRecomputeEvents | Represents a collection of assembly recompute events. | 
| Attribute | Represents an occurrence of a user-defined attribute. | 
| AttributeQuery | Contains the QueryByName method, which enables you to locate attribute sets and individual attributes. | 
| AttributeSet | Represents an occurrence of a user-defined attribute set. | 
| AttributeSets | Represents a collection of AttributeSet objects. | 
| BlockTableEvents | Contains the AfterUpdate event. | 
| Command | Provides interfaces for Visual Basic users to capture user input to process Solid Edge events. | 
| CommandBar | Represents all menus, toolbars, and pop-up menus in Solid Edge. | 
| CommandBarButton | Represents buttons on toolbars and menus. | 
| CommandBarButtonEvents | A collection of CommandBarButtonEvent objects. | 
| CommandBarControl | Contains the properties and methods that are applicable to both CommandBarButton and CommandBarPopup objects. | 
| CommandBarControls | Contains all of the buttons and pop-ups on a specific command bar. | 
| CommandBarPopup | Represents pop-ups on toolbars and menus. | 
| CommandBars | A collection of all of the command bars within a specific environment. | 
| CommandCategories | A collection of command categories | 
| CommandCategory |  | 
| CommandInfo |  | 
| CommandWindow | Triggers Command Window events. | 
| ConnectorTableEvents | Contains the AfterUpdate event. | 
| CPDInitializer |  | 
| CPDInitializerInsightXT |  | 
| Customization | An object that is sued to Customize the UI | 
| DashStyle | The DashStyle object represents a custom dash style in a Draft document. | 
| DashStyles | The DashStyles object represents a collection of DashStyle objects. | 
| DISEAddInEvents | A collection of AddInEvent objects. | 
| DISEAddInEventsEx | A collection of AddInEvent objects. | 
| DISEApplicationEvents | Fires application events. | 
| DISEApplicationWindowEvents | Provides access to the application window events. | 
| DISEAssemblyFamilyEvents |  | 
| DISEAssemblyRecomputeEvents | Represents a collection of assembly recompute events. | 
| DISECommand | Provides interfaces for Visual Basic users to capture user input to process Solid Edge events. | 
| DISECommandBarButtonEvents | A collection of CommandBarButtonEvent objects. | 
| DISECommandEvents |  | 
| DISECommandWindowEvents |  | 
| DISEDocumentEvents | Fires document events. | 
| DISEFileUIEvents | Fires file user interface events. | 
| DISEhDCDisplayEvents | Fires display events. | 
| DISEMouse | Provides interfaces for Visual Basic users to capture user input to process Solid Edge mouse events. | 
| DISEMouseEvents |  | 
| DISEViewEvents | Fires view events. | 
| DisplayEvents | Fires display events. | 
| DividePartEvents | Represents a collection of DividedPart-based events. | 
| DocumentEvents | Fires document events. | 
| Documents | A collection of Document objects. | 
| DraftBendTableEvents | Contains the AfterUpdate event. | 
| DrawingViewEvents | Represents a collection of DrawingView events. | 
| Environment | The menus and accelerators to a Window object.  Defines the set of commands that can be run while a window associated to an environment is active. | 
| Environments | A collection of Environment objects. | 
| FaceStyle | An object in the FaceStyles collection. | 
| FaceStyles | A collection of FaceStyle objects. | 
| FamilyOfPartsEvents | Represents a collection of Family of Parts events. | 
| FamilyOfPartsExEvents |  | 
| FeatureLibraryEvents | Represents a collection of Feature Library-based events. | 
| FileUIEvents | Fires file user interface events. | 
| FillStyle | Defines the fill characteristics of an enclosed object. | 
| FillStyles | A collection of FillStyle objects. | 
| GLDisplayEvents | Represents a collection of GLDisplay events. | 
| HatchPatternStyle | A vector pattern that is used to fill a closed boundary. | 
| HatchPatternStyles | A collection of HatchPatternStyle objects. | 
| HighlightSet | Represents an occurrence of a Highlight set in Assembly, Draft, Part, or Sheet Metal documents. | 
| HighlightSets | A collection of HighLightSet objects. | 
| Insight | Insight Automation Object | 
| InterpartLink |  | 
| InterpartLinks |  | 
| ISEAccelerator | Represents a collection of KeyBinding objects. | 
| ISEAccelerators | Represents a collection of Accelerator objects. | 
| ISEAddIn | A control that represents a command added to Solid Edge through the AddIn interface. | 
| ISEAddInEdgeBarEvents |  | 
| ISEAddInEdgeBarEventsEx |  | 
| ISEAddInEvents | A collection of AddInEvent objects. | 
| ISEAddInEventsEx | A collection of AddInEvent objects. | 
| ISEAddInEx | A control that represents a command added to Solid Edge through the AddIn interface. | 
| ISEAddIns | A collection of AddIn objects. | 
| ISEApplicationEvents | Fires application events. | 
| ISEApplicationV8AfterDocumentOpenEvent | Fires document open event | 
| ISEApplicationWindowEvents | Provides access to the application window events. | 
| ISEAssemblyFamilyEvents |  | 
| ISEAssemblyRecomputeEvents | Represents a collection of assembly recompute events. | 
| ISEBlockTableEvents | Contains the AfterUpdate event. | 
| ISECommand | Provides interfaces for Visual Basic users to capture user input to process Solid Edge events. | 
| ISECommandBar | Represents all menus, toolbars, and pop-up menus in Solid Edge. | 
| ISECommandBarButton | Represents buttons on toolbars and menus. | 
| ISECommandBarButtonEvents | A collection of CommandBarButtonEvent objects. | 
| ISECommandBarControl | Contains the properties and methods that are applicable to both CommandBarButton and CommandBarPopup objects. | 
| ISECommandBarControls | Contains all of the buttons and pop-ups on a specific command bar. | 
| ISECommandBarPopup | Represents pop-ups on toolbars and menus. | 
| ISECommandBars | A collection of all of the command bars within a specific environment. | 
| ISECommandCategories | A collection of command categories | 
| ISECommandCategory |  | 
| ISECommandEvents |  | 
| ISECommandEx | Provides interfaces for Visual Basic users to capture user input to process Solid Edge events. | 
| ISECommandInfo |  | 
| ISECommandWindowEvents |  | 
| ISEConnectorTableEvents | Contains the AfterUpdate event. | 
| ISEDividePartEvents | Represents a collection of DividedPart-based events. | 
| ISEDocumentEvents | Fires document events. | 
| ISEDraftBendTableEvents | Contains the AfterUpdate event. | 
| ISEDrawingViewEvents | Represents a collection of DrawingView events. | 
| ISEDynamicEditEvents | Fires dynamic edit events. | 
| ISEECEvents | SEEC Events | 
| ISEFamilyOfPartsEvents | Represents a collection of Family of Parts events. | 
| ISEFamilyOfPartsExEvents |  | 
| ISEFeatureLibraryEvents | Represents a collection of Feature Library-based events. | 
| ISEFileUIEvents | Fires file user interface events. | 
| ISEhDCDisplayEvents | Fires display events. | 
| ISEIGLDisplayEvents | Represents a collection of GLDisplay events. | 
| ISEKeyBinding | Provides information about an existing key binding. | 
| ISELocateFilterEvents |  | 
| ISEModelRecomputeEvents | Fires model recompute events. | 
| ISEMouse | Provides interfaces for Visual Basic users to capture user input to process Solid Edge mouse events. | 
| ISEMouseEvents |  | 
| ISEMouseEx |  | 
| ISENewFileUIEvents |  | 
| ISEPartsListEvents | Contains the AfterUpdate event. | 
| ISERenderEvents | Represents a collection of rendering events. | 
| ISEShortCutMenuEvents | Event set for short-cut menu manipulations | 
| ISEViewEvents | Fires view events. | 
| ISolidEdgeAddIn | Provides an interface for add-ins to implement for Solid Edge to connect to them. | 
| ISolidEdgeBar |  | 
| ISolidEdgeBarEx |  | 
| ISolidEdgeBarEx2 |  | 
| ISolidEdgeCommandBar |  | 
| ISolidEdgeRibbonBar |  | 
| ISolidEdgeRibbonBarEx |  | 
| KeyBinding | Provides information about an existing key binding. | 
| Layer | An object in the Layers collection object. | 
| Layers | A collection of Layer objects. | 
| LinearStyle | Consists of the information required to represent a line graphically. | 
| LinearStyles | A collection of LinearStyle objects. | 
| MatTable |  | 
| ModelRecomputeEvents | Fires model recompute events. | 
| Mouse | Provides interfaces for Visual Basic users to capture user input to process Solid Edge mouse events. | 
| NewFileUIEvents |  | 
| PartsListEvents | Contains the AfterUpdate event. | 
| Properties | A collection of Property objects. | 
| Property | A user-defined document attribute. | 
| PropertySets | A collection of PropertySet objects. | 
| QueryObjects | Represents the collection of objects returned by a query. | 
| RadialMenu |  | 
| Reference | Represents an object that references another object (a part or assembly, for example). | 
| RenderEvents | Represents a collection of rendering events. | 
| RibbonBar |  | 
| RibbonBarControl |  | 
| RibbonBarControls |  | 
| RibbonBarGroup |  | 
| RibbonBarGroups |  | 
| RibbonBars |  | 
| RibbonBarTab |  | 
| RibbonBarTabs |  | 
| RibbonBarTheme |  | 
| RibbonBarThemes |  | 
| RoutingSlip | Distributes a document to recipients either at one time or sequentially. | 
| SectionView | Automation object for a section view in a Part or Assembly document. | 
| SectionViews | Collection of section views. | 
| SEECEvents | SEEC Events | 
| SEGenericCollection | Represents a collection of AttachedProperty objects. | 
| SelectSet | A temporary grouping of one or more selected objects. | 
| Sensor | Represents an occurrence of a Sensor feature in an Assembly document, a Part document, or a Sheet Metal document. | 
| Sensors | A collection of Sensor objects. | 
| SheetMetalSensors | Represents a collection of sensors on a SheetMetalDocument. | 
| ShortcutMenuEvents |  | 
| SolidEdgeDocument |  | 
| SolidEdgeInsightXT | InsightXT Automation Object. | 
| SolidEdgeTCE |  | 
| SummaryInfo | Contains information about a document. | 
| SwitchWindowCust |  | 
| Symbol2d | Allows you to review or manipulate the symbol geometry, the attachment between a symbol and a source document, and the user property. | 
| SymbolProperties | A collection of SymbolProperty objects. | 
| Symbols | A collection of Symbol objects. | 
| TextCharStyle | Contains a set of character characteristics that can be applied as a set to the active text. | 
| TextCharStyles | A collection of TextCharStyle objects. | 
| TextStyle | Contains characteristics to apply to the active paragraph. | 
| TextStyles | A collection of TextStyle objects. | 
| UnitOfMeasure | The UnitOfMeasure object allows you to set and return the unit type and precision for each category, depending on the index of the unit. | 
| UnitsOfMeasure | Allows you to convert internal measurement units to user-specified measurement units. | 
| variable | Associates a name with a numeric value. | 
| VariableList | A list of Variable objects returned from a query. | 
| Variables | A collection of Variable objects. | 
| View | Provides methods and properties that allow you to manipulate Solid Edge window views. | 
| ViewEvents | Fires view events. | 
| ViewStyle | Contains a collection of properties that control view rendering. | 
| ViewStyles | A collection of ViewStyle objects. | 
| Window | Provides support for adjusting the size of the actual viewing area. | 
| Windows | A collection of Window objects. |