Solid Edge Framework Type Library
OnCommand Event
Collapse All
Expand All
Solid Edge Framework Type Library
>
AddInEvents Object
: OnCommand Event
The ID of the command for which the event is triggered.
Description
Occurs when the user selects the button for the associated add-in.
Syntax
Visual Basic
Public Event OnCommand( _ ByVal
nCmdID
As Long _ )
Parameters
nCmdID
The ID of the command for which the event is triggered.
See Also
AddInEvents Object
|
AddInEvents Members
Send comments
on this topic.