Solid Edge Framework Type Library
AfterCommandRun Event
Specifies the ID of the command for which the event is triggered.
Description
Occurs after a specified command is run.
Syntax
Visual Basic
Public Event AfterCommandRun( _
   ByVal theCommandID As Long _
)
Parameters
theCommandID
Specifies the ID of the command for which the event is triggered.
See Also

ApplicationEvents Object  | ApplicationEvents Members

Send comments on this topic.