Solid Edge Framework Type Library
Name Property
Description
Returns the name of the referenced object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Name As String
Remarks
All objects have names that are unique within the scope of their parent.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objBaseProfile(1 To 2) As SolidEdgePart.Profile
    Dim objLine1 As SolidEdgeFrameworkSupport.Line2d
    Dim objLine2 As SolidEdgeFrameworkSupport.Line2d
    Dim objArc1 As SolidEdgeFrameworkSupport.Arc2d
    Dim objArc2 As SolidEdgeFrameworkSupport.Arc2d
    Dim objModel As SolidEdgePart.Model
    Dim objExtProtrusion As SolidEdgePart.ExtrudedProtrusion
    Dim objRelations As SolidEdgeFrameworkSupport.Relations2d
    Dim objAttributeSet As Object
    Dim objAttribute As Object
    Const ATTRIBNAME = "My Attribute"
    Dim lngStatus As Long
    Dim strName As String


    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create an Extruded Protrusion as Base feature
    Set objBaseProfile(1) = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1))
    Set objLine1 = objBaseProfile(1).Lines2d.AddBy2Points(x1:=0.05, y1:=0, x2:=0.05, y2:=0.15)
    Set objArc1 = objBaseProfile(1).Arcs2d.AddByCenterStartEnd(xCenter:=0.025, yCenter:=0.15, _
                                                               xStart:=0.05, yStart:=0.15, xEnd:=0, yEnd:=0.15)
    Set objLine2 = objBaseProfile(1).Lines2d.AddBy2Points(x1:=0, y1:=0.15, x2:=0, y2:=0)
    Set objArc2 = objBaseProfile(1).Arcs2d.AddByCenterStartEnd(xCenter:=0.025, yCenter:=0, _
                                                               xStart:=0, yStart:=0, xEnd:=0.05, yEnd:=0)
    Set objRelations = objBaseProfile(1).Relations2d
    objRelations.AddKeypoint Object1:=objLine1, Index1:=igLineEnd, Object2:=objArc1, Index2:=igArcStart
    objRelations.AddKeypoint Object1:=objArc1, Index1:=igArcEnd, Object2:=objLine2, Index2:=igLineStart
    objRelations.AddKeypoint Object1:=objLine2, Index1:=igLineEnd, Object2:=objArc2, Index2:=igArcStart
    objRelations.AddKeypoint Object1:=objArc2, Index1:=igArcEnd, Object2:=objLine1, Index2:=igLineStart
    lngStatus = objBaseProfile(1).End(ValidationCriteria:=igProfileClosed)
    If lngStatus <> 0 Then
        MsgBox ("Base feature profile is not closed")
    End If

    Set objModel = objDoc.Models.AddFiniteExtrudedProtrusion(NumberOfProfiles:=1, ProfileArray:=objBaseProfile, _
                                                             ProfilePlaneSide:=igRight, ExtrusionDistance:=0.05)
    objBaseProfile(1).Visible = False
    Set objExtProtrusion = objModel.ExtrudedProtrusions(1)
    If objExtProtrusion.Status <> igFeatureOK Then
        MsgBox "Base Feature is not created properly"
    End If

    'Create an AttributeSet with Add method
    Set objAttributeSet = objExtProtrusion.AttributeSets.Add("MyAttrib Set")
    'Add an Attribute to the set with Add method
    Set objAttribute = objAttributeSet.Add(ATTRIBNAME, vbInteger)
    'Get the name of the Attribute
    strName = objAttribute.Name
    If strName <> ATTRIBNAME Then
        MsgBox "Name property returned wrong value"
    End If


    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objBaseProfile(1) = Nothing
    Set objBaseProfile(2) = Nothing
    Set objLine1 = Nothing
    Set objLine2 = Nothing
    Set objArc1 = Nothing
    Set objArc2 = Nothing
    Set objModel = Nothing
    Set objExtProtrusion = Nothing
    Set objRelations = Nothing
    Set objAttributeSet = Nothing
    Set objAttribute = Nothing
End Sub
See Also

Attribute Object  | Attribute Members

Send comments on this topic.