Application | Returns the active application object. |
BeginGroup | Specifies whether or not a button has a dividing bar on its left-hand side. |
BuiltIn | Specifies whether the control is a built-in command or a standard Solid Edge commnd. |
BuiltInFace | Returns whether or not the current face is the control’s built-in face. |
Caption | Sets and returns the caption of the referenced object. |
CommandBarButtonEvents | Returns a CommandBarButtonEvents object. |
DescriptionText | Sets and returns the description of the referenced button. |
Enabled | Specifies whether or not the specified object is enabled. |
FaceId | Defines the ID number for the button face of the referenced object. |
Height | Returns the height of the referenced object. |
HelpContextId | Sets or returns the Help Context ID number for the Help topic that is attached to the referenced object. |
HelpFile | Sets or returns the Help file that is attached to the referenced object. |
Id | Returns the ID for the referenced built-in command bar control. |
Index | Returns the numeric index for the active object. |
Left | Specifies the distance (in twips) between the internal left edge of an object and the left edge of its container. |
OnAction | Sets or returns the name of the macro to run when the user clicks a command bar control or when the Execute method on the control is run. |
ParameterText | Sets or returns the parameters used by Solid Edge when running built-in controls. |
Parent | Returns the parent object for the referenced object. |
ShortcutText | Defines the shortcut key text that is displayed next to the referenced button control. |
State | Defines the current state of the referenced button. |
Style | For collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only. |
Tag | Defines information about the referenced control. |
TooltipText | Sets and returns the string to be used as the tooltip for the referenced control. |
Top | Sets and returns the distance from the top of the screen to the top of the referenced object or control. |
Type | Specifies the type of the object being referenced. |
Visible | Specifies whether or not the referenced object is displayed to the screen. |
Width | Returns the width of the referenced object. |