Solid Edge Framework Type Library
DescriptionText Property
Collapse All
Expand All
Solid Edge Framework Type Library
>
CommandBarPopup Object
: DescriptionText Property
Description
Sets and returns the description of the referenced button.
Property type
Read-write property
Syntax
Visual Basic
Public Property DescriptionText As String
Remarks
The description is displayed in the status bar of the container application when the user positions the pointer over a command bar control.
See Also
CommandBarPopup Object
|
CommandBarPopup Members
Send comments
on this topic.