Solid Edge Framework Type Library
OnAction Property
Collapse All
Expand All
Solid Edge Framework Type Library
>
CommandBarPopup Object
: OnAction Property
Description
Sets or returns the name of the macro to run when the user clicks a command bar control or when the Execute method on the control is run.
Property type
Read-write property
Syntax
Visual Basic
Public Property OnAction As String
See Also
CommandBarPopup Object
|
CommandBarPopup Members
Send comments
on this topic.