Solid Edge Framework Type Library
Enabled Property
Collapse All
Expand All
Solid Edge Framework Type Library
>
CommandBar Object
: Enabled Property
Description
Specifies whether or not the specified object is enabled.
Property type
Read-write property
Syntax
Visual Basic
Public Property Enabled As Boolean
Remarks
Setting this property to True causes the name of the command bar to appear in the list of available command bars.
See Also
CommandBar Object
|
CommandBar Members
Send comments
on this topic.