| Solid Edge Framework Type Library : Customization Object |
BeginCustomization | Must call this method at the start of customization. |
EndCustomization | Must call this method at the end of customization to free up resources. |
Application | Returns the active application object. |
Parent | Returns the parent object for the referenced object. |
RadialMenu | Returns the RadialMenus collection object, which is used to customize the radial menu layout. |
RibbonBarThemes | Returns the RibbonBarThemes collection object, which is used to customize the ribbon bar layout. |
SwitchWindowCust | Returns the SwitchWindow collection object. |