|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  Center | This read-write Boolean property sets and returns whether the referenced DashStyle object represents a repeated pattern.  The property is True if the pattern is not repeated, and False if the pattern is repeated. | 
|  DashGapCount | Returns the number of dashes and gaps in the dash definition. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  Name | Returns the name of the referenced object. | 
|  PercentStartEndDash | This read-write Double property sets and returns the percentage of the first and last dash drawn for the referenced DashStyle object. | 
|  Units | Sets and returns the units in which the line width is defined. |