Solid Edge Framework Type Library
AfterDividePartDocumentRenamed Event
Description
Occurs when the interactive Rename command is run on a DividedPart or when the DividedPart.DocumentName property changes.
Syntax
Visual Basic
Public Event AfterDividePartDocumentRenamed( _
   ByVal theMember As Object, _
   ByVal OldName As String _
)
Parameters
theMember
OldName
See Also

DividePartEvents Object  | DividePartEvents Members

Send comments on this topic.