The menus and accelerators to a Window object. Defines the set of commands that can be run while a window associated to an environment is active.
Object Model
Remarks
The environment describes the menus and accelerators to the window. Additionally, the environment defines the set of commands that can be executed while a window associated to an environment is active. An environment is associated with zero to many windows.