Changes the color of each hatch line in the referenced HatchPatternStyle object.
Syntax
Visual Basic
Public Sub SetMasterColor( _
ByVal nColor As Long _
)
Parameters
nColor
Specifies the color to apply.
Remarks
It is equivalent to calling the SetColor method for each hatch line in the pattern. The color is stored in a long integer, created with the RGB function (red, green, and blue color intensities), or as an integer between 0 and 15 representing standard colors.