Specifies the display index (sequence number in which the linear element was created) for the linear element.
Specifies the new angle of rotation for the linear element. The angle is measured counterclockwise from the horizontal for positive angles. The angular units are the active angular readout unit.
Description
Specifies a new angle of rotation for a specified linear element used in a HatchPatternStyle object.
Specifies the display index (sequence number in which the linear element was created) for the linear element.
dRotation
Specifies the new angle of rotation for the linear element. The angle is measured counterclockwise from the horizontal for positive angles. The angular units are the active angular readout unit.