Solid Edge Framework Type Library
Help Method
The handle to the Application frame window.
Specifies the type of search the help is to perform.
Description
Displays help for the referenced control.
Syntax
Visual Basic
Public Function Help( _
   ByVal hFrameWnd As Long, _
   ByVal HelpCommandID As Long _
) As HResult
Parameters
hFrameWnd
The handle to the Application frame window.
HelpCommandID
Specifies the type of search the help is to perform.
See Also

ISECommandBarButtonEvents Object  | ISECommandBarButtonEvents Members

Send comments on this topic.