Solid Edge Framework Type Library
BuiltInFace Property
Collapse All
Expand All
Solid Edge Framework Type Library
>
ISECommandBarControl Object
: BuiltInFace Property
Description
Returns whether or not the current face is the control’s built-in face.
Property type
Read-write property
Syntax
Visual Basic
Public Property BuiltInFace As Boolean
Remarks
If True, the face of the button is its built-in face. This property can only be set to True, which will reset the face to the built-in one.
See Also
ISECommandBarControl Object
|
ISECommandBarControl Members
Send comments
on this topic.