Solid Edge Framework Type Library
Execute Method
Collapse All
Expand All
Solid Edge Framework Type Library
>
ISECommandBarControl Object
: Execute Method
Description
Runs either the built-in command that is assigned to the referenced button or the macro defined by the OnAction property.
Syntax
Visual Basic
Public Function Execute() As HResult
See Also
ISECommandBarControl Object
|
ISECommandBarControl Members
Send comments
on this topic.