Solid Edge Framework Type Library
Left Property
Collapse All
Expand All
Solid Edge Framework Type Library
>
ISECommandBarControl Object
: Left Property
Description
Specifies the distance (in twips) between the internal left edge of an object and the left edge of its container.
Property type
Read-only property
Syntax
Visual Basic
Public Property Left As Long
See Also
ISECommandBarControl Object
|
ISECommandBarControl Members
Send comments
on this topic.