Solid Edge Framework Type Library
Top Property
Collapse All
Expand All
Solid Edge Framework Type Library
>
ISECommandBarControl Object
: Top Property
Description
Sets and returns the distance from the top of the screen to the top of the referenced object or control.
Property type
Read-only property
Syntax
Visual Basic
Public Property Top As Long
Remarks
Returns the distance (in pixels) from the top edge of the control to the top of the screen.
See Also
ISECommandBarControl Object
|
ISECommandBarControl Members
Send comments
on this topic.