|  Application | Returns the active application object. | 
|  BuiltIn | Specifies whether the control is a built-in command or a standard Solid Edge commnd. | 
|  Controls | Returns the CommandBarControls object that contains the buttons associated with the referenced object. | 
|  Enabled | Specifies whether or not the specified object is enabled. | 
|  Height | Returns the height of the referenced object. | 
|  Index | Returns the numeric index for the active object. | 
|  Left | Specifies the distance (in twips) between the internal left edge of an object and the left edge of its container. | 
|  Name | Returns the name of the referenced object. | 
|  NameLocal | Sets and returns the name of a command bar as it is displayed in the language version of Solid Edge. | 
|  Parent | Returns the parent object for the referenced object. | 
|  Position | Sets and returns the position of the referenced CommandBar object. | 
|  Top | Sets and returns the distance from the top of the screen to the top of the referenced object or control. | 
|  Type | Specifies the type of the object being referenced. | 
|  Visible | Specifies whether or not the referenced object is displayed to the screen. | 
|  Width | Returns the width of the referenced object. |