Solid Edge Framework Type Library
ISECommandInfo Object Members
Overview
Collapse All
Expand All
Solid Edge Framework Type Library
: ISECommandInfo Object
Public Properties
BuiltIn
Specifies whether the control is a built-in command or a standard Solid Edge commnd.
Caption
Returns the name of the referenced object.
Description
Icon
Id
Returns the ID for the referenced built-in command bar control.
Tooltip
See Also
ISECommandInfo Object
|
Solid Edge ST - What's New
Send comments
on this topic.