Solid Edge Framework Type Library
AfterDividePartDocumentCreated Method
Specifies the object for which the event is triggered.
Description
Occurs when Populate is called (and succeeds) for a Divided Part.
Syntax
Visual Basic
Public Function AfterDividePartDocumentCreated( _
   ByVal theMember As Object _
) As HResult
Parameters
theMember
Specifies the object for which the event is triggered.
See Also

ISEDividePartEvents Object  | ISEDividePartEvents Members

Send comments on this topic.