Solid Edge Framework Type Library
ActivateInContext Method
Collapse All
Expand All
Solid Edge Framework Type Library
>
Layer Object
: ActivateInContext Method
Required Object (input). Specifies the sheet on which to activate the layer.
Description
This method activates the referenced Layer object on the specified sheet.
Syntax
Visual Basic
Public Sub ActivateInContext( _ ByVal
Context
As Object _ )
Parameters
Context
Required Object (input). Specifies the sheet on which to activate the layer.
See Also
Layer Object
|
Layer Members
Send comments
on this topic.