Sets and returns the locate mode for the referenced object.
Property type
Read-write property
Syntax
Visual Basic
Public Property LocateMode As Long
Remarks
A value of 0 implies SmartMouse locate, 1 implies simple click locate (no multi-select dialog), 2 implies quick pick locate (multi-select dialog where applicable), and 3 implies no locate (used to receive mouse events without performing any locate). For simple and QuickPick locate modes, users can mouse down, drag, and mouse up for fence locate. This property is applicable when a mouse service object is registered.