| Solid Edge Framework Type Library : RadialMenu Collection |
Commit | Commits all pending changes to all RadialMenu and child items. |
Create | Creates a new RibbonBarTheme from an existing RibbonBarTheme. Accepts a string or RibbonBarTheme as input. |
DumpPallet | Dumps the Radial Menu Pallet for the given environment to the given logfile. |
DumpPallets | Dumps the Radial Menu Pallets to the given logfile. |
Item | Returns an item in the collection. Valid inputs are a positive or negative integer index or the string name of the item. |
LoadPallets | Loads the Radial Menu Pallets. |
Remove | Removes the theme from this collection. |
RemoveCommand | Removes the command on the given wedge of the given ring of the Radial Menu Pallet for the given environment. |
SavePallets | Saves the Radial Menu Pallets. |
SetCommand | Set the command on the given wedge of the given ring of the Radial Menu Pallet for the given environment. |
SwapCommands | Swaps the commands on the given wedges of the given rings of the Radial Menu Pallet for the given environment. |
Application | Returns the active application object. |
Count | Returns the number of objects in the referenced collection. |
Parent | Returns the parent object for the referenced object. |