Solid Edge Framework Type Library
GetMatrix Method
Collapse All
Expand All
Solid Edge Framework Type Library
>
Reference Object
: GetMatrix Method
Returns the 4x4 array that specifies the position and orientation of the part. This is a single-dimension Double array that contains 16 elements.
Description
Returns the transformation matrix for the referenced Occurrence or Reference object.
Syntax
Visual Basic
Public Sub GetMatrix( _ ByRef
Matrix
() As Double _ )
Parameters
Matrix
Returns the 4x4 array that specifies the position and orientation of the part. This is a single-dimension Double array that contains 16 elements.
Remarks
This matrix defines the current position and orientation of the object.
See Also
Reference Object
|
Reference Members
Send comments
on this topic.