Solid Edge Framework Type Library
Add Method
Number of profiles.
Array of profiles.
Caption for view.
Description
Adds a section view to the collection.
Syntax
Visual Basic
Public Function Add( _
   ByVal nNumProfiles As Long, _
   ByRef pProfiles() As Unknown, _
   ByVal szCaption As String, _
   ByVal dExtent As Double, _
   ByVal eExtentSide As SectionViewExtentSide, _
   ByVal eProfileSide As SectionViewProfileSide, _
   ByVal bCutHardwareParts As Long _
) As Object
Parameters
nNumProfiles
Number of profiles.
pProfiles
Array of profiles.
szCaption
Caption for view.
dExtent
eExtentSide
ValueDescription
igFiniteSymmetricExtentFinite symmetric extent side.
igInfiniteLeftExtentInfinite left extent side.
igInfiniteRightExtentInfinite right extent side.
igLeftExtentLeft extent side.
igRightExtentRight extent side.
igThroughAllExtentThrough all extent side.
eProfileSide
ValueDescription
igInsideProfileSideInside profile side.
igLeftProfileSideLeft profile side.
igOutsideProfileSideOutside profile side.
igRightProfileSideRight profile side.
bCutHardwareParts
Example
Private Sub btnSection_Click(sender As System.Object, e As System.EventArgs) Handles btnPMIModelSection.Click
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim asmDoc As SolidEdgeAssembly.AssemblyDocument = Nothing
        Dim layout As SolidEdgeAssembly.Layout = Nothing
        Dim profileArray(0 To 0) As SolidEdgePart.Profile

        Try
            'Create/get the application with specific settings PMIModelView 
            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            asmDoc = objApplication.ActiveDocument
            layout = asmDoc.Layouts.Add(asmDoc.AsmRefPlanes.Item(3))
            profileArray(0) = layout.Profile

            Call profileArray(0).Lines2d.AddBy2Points(0, -1, 0, 1)

            Dim sectionViews As SolidEdgeFramework.SectionViews = asmDoc.SectionViews
            Dim sectionView As SolidEdgeFramework.SectionView = sectionViews.Add(1, profileArray, "test", 0.05, SolidEdgeFramework.SectionViewExtentSide.igLeftExtent, SolidEdgeFramework.SectionViewProfileSide.igRightProfileSide, False)

            Call sectionView.Show(False)
            Call sectionView.Show(True)

            Dim caption As String = sectionView.Caption

            sectionView.Caption = "Caption"

            Call sectionView.Delete()
        Catch ex As Exception
            MsgBox(ex.ToString)
        End Try
    End Sub
See Also

SectionViews Collection  | SectionViews Members  | Solid Edge ST5 - What's New

Send comments on this topic.