Solid Edge Framework Type Library
Add Method
Specifies the object to be added to the selection set.
Description
Adds an occurrence of the referenced object.
Syntax
Visual Basic
Public Sub Add( _
   ByVal Dispatch As Object _
) 
Parameters
Dispatch
Specifies the object to be added to the selection set.
Remarks
As of Solid Edge V17 build 28, the Add() method will now take in a HighlightSet collection object.
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objDocuments As SolidEdgeFramework.Documents = Nothing
        Dim objSelectSet As SolidEdgeFramework.SelectSet = Nothing
        Dim objAssemblyDocument As SolidEdgeAssembly.AssemblyDocument = Nothing
        Dim objOccurrences As SolidEdgeAssembly.Occurrences = Nothing
        Dim objOccurrence As SolidEdgeAssembly.Occurrence = Nothing
        Dim objHighlightSets As SolidEdgeFramework.HighlightSets = Nothing
        Dim objHighlightSet As SolidEdgeFramework.HighlightSet = Nothing
        Dim objTrainingFolder As DirectoryInfo
        Dim objFileInfo As FileInfo
        Dim i As Integer

        Try
            OleMessageFilter.Register()

            objTrainingFolder = GetTrainingFolder()
            objFileInfo = New FileInfo(Path.Combine(objTrainingFolder.FullName, "Try It\BrakePedalAssy.asm"))
            objApplication = Activator.CreateInstance(Type.GetTypeFromProgID("SolidEdge.Application"))
            objApplication.Visible = True
            objDocuments = objApplication.Documents
            objAssemblyDocument = objDocuments.Open(objFileInfo.FullName)
            objHighlightSets = objAssemblyDocument.HighlightSets
            objSelectSet = objApplication.ActiveSelectSet
            objOccurrences = objAssemblyDocument.Occurrences

            ' Add individual Occurrence objects to SelectSet.
            ' This method can cause significant GUI performance problems
            ' because the screen redraws after each Add() call.
            For i = 1 To objOccurrences.Count
                objSelectSet.Add(objOccurrences.Item(i))
            Next

            ' Clear the SelectSet.
            objSelectSet.RemoveAll()

            ' Create a new HighlightSet
            objHighlightSet = objHighlightSets.Add()

            ' Demonstrate adding HighlightSet to SelectSect (Added in V17).
            For i = 1 To objOccurrences.Count
                objHighlightSet.AddItem(objOccurrences.Item(i))
            Next

            ' Add entire HighlightSet to SelectSet.
            ' This is the fastest way to add a large collection of objects.
            objSelectSet.Add(objHighlightSet)
        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub

    Function GetTrainingFolder() As DirectoryInfo
        Dim objInstallData As SEInstallDataLib.SEInstallData = Nothing
        Dim objInstallFolder As DirectoryInfo = Nothing
        Dim objTrainingFolder As DirectoryInfo = Nothing

        Try
            objInstallData = New SEInstallDataLib.SEInstallData
            objInstallFolder = New DirectoryInfo(objInstallData.GetInstalledPath())
            objTrainingFolder = New DirectoryInfo(Path.Combine(objInstallFolder.Parent.FullName, "Training"))
        Catch
        Finally
            If Not (objInstallData Is Nothing) Then
                Marshal.FinalReleaseComObject(objInstallData)
                objInstallData = Nothing
            End If
        End Try

        Return objTrainingFolder
    End Function
End Module
See Also

SelectSet Collection  | SelectSet Members

Send comments on this topic.