Solid Edge Framework Type Library
RemoveAll Method
Description
Removes all objects from the referenced object.
Syntax
Visual Basic
Public Sub RemoveAll() 
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objSelectSet As SolidEdgeFramework.SelectSet
    Dim objProfile As SolidEdgePart.Profile
    Dim objLine1 As SolidEdgeFrameworkSupport.Line2d
    Dim objLine2 As SolidEdgeFrameworkSupport.Line2d
    Dim objCircle1 As SolidEdgeFrameworkSupport.Circle2d
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create few 2d elements
    Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1))
    Set objLine1 = objProfile.Lines2d.AddBy2Points(x1:=0, y1:=0, x2:=0.1, y2:=0.1)
    Set objLine2 = objProfile.Lines2d.AddBy2Points(x1:=0, y1:=0, x2:=0, y2:=0.1)
    Set objCircle1 = objProfile.Circles2d.AddByCenterRadius(x:=0, y:=0, Radius:=0.05)
    'Get SelectSet object from the PartDocument
    Set objSelectSet = objDoc.SelectSet
    'Add a line and circle to the selectset
    Call objSelectSet.Add(dispatch:=objLine1)
    Call objSelectSet.Add(dispatch:=objCircle1)
    'Remove All elements from the selectset
    objSelectSet.RemoveAll
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSelectSet = Nothing
    Set objLine1 = Nothing
    Set objLine2 = Nothing
    Set objCircle1 = Nothing
End Sub
See Also

SelectSet Collection  | SelectSet Members

Send comments on this topic.