AttributeSets | Returns the AttributeSets collection object for the referenced object. |
CurrentValue | Returns the current value of the referenced Sensor object. |
Description | Returns a user-specified description of the referenced object. |
DisplayType | Sets and returns the display type of the referenced Sensor object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
IsInRange | Returns whether the current value of the referenced Sensor object is within the specified range. |
LowerRange | Sets and returns the lower range of the referenced Sensor object. |
MaximumThreshold | Sets and returns the maximum threshold of the referenced Sensor object. |
MinimumThreshold | Sets and returns the minimum threshold of the referenced Sensor object. |
Name | Returns the name of the referenced object. |
Operator | Sets and returns the logical operator of the referenced Sensor object. |
SensorType | Returns the sensor type of the referenced Sensor object. |
Status | Returns the status of the specified object. |
UpdateMechanism | Sets and returns the update mechanism of the referenced Sensor object. |
UpperRange | Sets and returns the upper range of the referenced Sensor object. |