| Solid Edge Framework Type Library > SheetMetalSensors Collection : AddVariableSensor Method |
| Visual Basic |
|---|
Public Function AddVariableSensor( _ ByVal variable As Object, _ ByVal Name As String, _ ByVal Description As String, _ ByVal LowerRange As Double, _ ByVal UpperRange As Double, _ ByVal MinimumThreshold As Double, _ ByVal MaximumThreshold As Double, _ ByVal Operator As SensorOperatorConstants, _ ByVal DisplayType As SensorDisplayTypeConstants, _ ByVal UpdateMechanism As SensorUpdateMechanismConstants _ ) As Object |
| Value | Description |
|---|---|
| seSensorOperatorBetween | Sensor operator - between |
| seSensorOperatorEqualTo | Sensor operator - equal to |
| seSensorOperatorGreaterThan | Sensor operator - greater than |
| seSensorOperatorInvalid | Invalid sensor operator |
| seSensorOperatorLessThan | Sensor operator - less than |
| seSensorOperatorNotBetween | Sensor operator - not between |
| seSensorOperatorNotEqualTo | Sensor operator - not equal to |
| Value | Description |
|---|---|
| seSensorDisplayTypeHorizontalRange | Sensor display - horizontal range |
| seSensorDisplayTypeInvalid | Invalid sensor display |
| seSensorDisplayTypeTrueFalse | Sensor display - true/false |
| Value | Description |
|---|---|
| seSensorUpdateMechanismAutomatic | Automatic sensor update |
| seSensorUpdateMechanismInvalid | Invalid sensor update mechanism |
| seSensorUpdateMechanismManual | Manual sensor update |