| Solid Edge Framework Type Library > SolidEdgeInsightXT Object : DownladDocumentsFromServerWithOptions Method |
It is a Boolean flag. It has following possible values:
A Boolean flag which will decide the download level of the file.
| Visual Basic |
|---|
Public Sub DownladDocumentsFromServerWithOptions( _ ByVal bstrItemId As String, _ ByVal bstrItemRev As String, _ ByVal bstrDataSetFileName As String, _ ByVal bstrRevisionRule As String, _ ByVal bstrVariantRule As String, _ ByVal vbReadOnly As Boolean, _ ByVal vbAllLevel As Boolean, _ ByVal dwDownloadOption As ULong, _ Optional ByRef pvarListOfFiles() As Variant _ ) |
It is a Boolean flag. It has following possible values:
A Boolean flag which will decide the download level of the file.
Private Sub Command1_Click() On Error Resume Next Dim objApplication As SolidEdgeFramework.Application Dim objSolidEdgeInsightXT As SolidEdgeFramework.SolidEdgeInsightXT Set objApplication = GetObject(, "SolidEdge.Application") Set objSolidEdgeInsightXT = objApplication.SolidEdgeInsightXT Dim FileItemID As String Dim FileItemRevID As String Dim FileDataSetName As String Dim FileRevisionRule As String Dim FileVariantRule As String Dim vbreadonly As Boolean Dim vballlevel As Boolean Dim dwDownloadOption As Integer FileItemID = "020147" FileItemRevID = "A" FileDataSetName = "020147.par" FileRevisionRule = "latest working" FileVariantRule = "" vbreadonly = True vballlevel = False Call objSolidEdgeInsightXT.DownladDocumentsFromServerWithOptions(FileItemID, _ FileItemRevID, _ FileDataSetName, _ FileRevisionRule, _ FileVariantRule, _ vbreadonly, _ vballlevel, _ dwDownloadOption) Set objSolidEdgeInsightXT = Nothing Set objApplication = Nothing End Sub