Solid Edge Framework Type Library
OnSynchronizeFile Method
The variant array which contains the file list to be Synchronize.
Description
Synchronize files from cache
Syntax
Visual Basic
Public Sub OnSynchronizeFile( _
   ByRef psaSynchFiles() As Variant, _
   Optional ByVal enumSyncOption As SyncOption = SEECSyncAll _
) 
Parameters
psaSynchFiles
The variant array which contains the file list to be Synchronize.
enumSyncOption
ValueDescription
SEECSyncAll 
SEECSyncOne 
Example
Private Sub Command1_Click()
    On Error Resume Next
    Dim objApplication As SolidEdgeFramework.Application
    Dim objSolidEdgeInsightXT  As SolidEdgeFramework.SolidEdgeInsightXT
    
    Set objApplication = GetObject(, "SolidEdge.Application")
    Set objSolidEdgeInsightXT = objApplication.SolidEdgeInsightXT

    Dim varInputList(1) As Variant
    varInputList(0) = "F:\016954.asm"
    varInputList(1) = "F:\016973.asm"
    Call objSolidEdgeInsightXT.OnSynchronizeFile(varInputList)

    Set objSolidEdgeInsightXT = Nothing
    Set objApplication = Nothing
End Sub
See Also

SolidEdgeInsightXT Object  | SolidEdgeInsightXT Members  | Solid Edge ST4 - What's New

Send comments on this topic.