| Solid Edge Framework Type Library > SolidEdgeInsightXT Object : SetInsightXTMode Method |
A boolean flag which is used to specify whether to make the InsightXT Mode ON\OFF.
It has two possible values:
| Visual Basic |
|---|
Public Sub SetInsightXTMode( _ ByVal bMode As Boolean _ ) |
A boolean flag which is used to specify whether to make the InsightXT Mode ON\OFF.
It has two possible values:
Private Sub Command1_Click() On Error Resume Next Dim objApplication As SolidEdgeFramework.Application Dim objSolidEdgeInsightXT As SolidEdgeFramework.SolidEdgeInsightXT Set objApplication = GetObject(, "SolidEdge.Application") Set objSolidEdgeInsightXT = objApplication.SolidEdgeInsightXT Dim bMode As Boolean bMode = True Call objSolidEdgeInsightXT.SetInsightXTMode(bMode) Set objSolidEdgeInsightXT = Nothing Set objApplication = Nothing End Sub