Solid Edge Framework Type Library
DeleteFilesFromCache Method
The variant array which contains the file list to be Deleted from Cache.
Description
Deletes files in the cache
Syntax
Visual Basic
Public Sub DeleteFilesFromCache( _
   ByRef psaCacheFiles() As Variant _
) 
Parameters
psaCacheFiles
The variant array which contains the file list to be Deleted from Cache.
Example
Option Explicit

Sub Example()
    Dim objApplication As SolidEdgeFramework.Application
    Dim objTCE As SolidEdgeFramework.SolidEdgeTCE
    Dim varInputList(1) As Variant

    Set objApplication = GetObject(, "SolidEdge.Application")
    Set objTCE = objApplication.SolidEdgeTCE

    varInputList(0) = "F:\020042.par"
    varInputList(1) = "F:\020043.asm"
    
    Call objTCE.DeleteFilesFromCache(varInputList)

    If Not objApplication Is Nothing Then
        Call objApplication.Quit
    End If
    
    Set objTCE = Nothing
    Set objApplication = Nothing
End Sub
See Also

SolidEdgeTCE Object  | SolidEdgeTCE Members  | Solid Edge V20 - What's New  | Solid Edge V19 SP2 - What's New

Send comments on this topic.