| Solid Edge Framework Type Library > SolidEdgeTCE Object : GetSEECOrTCPreferenceValues Method | 
This is two dimensional array. Each row represents preference information. Each column will contain in and out information.
|  | Please note that caller should create two dimensional array with 2 columns otherwise API fails with invalid argument. The caller should provide preference names in first column only. | 
| Visual Basic | 
|---|
| Public Sub GetSEECOrTCPreferenceValues( _ ByRef pvarPreferenceInfo As Variant _ ) | 
This is two dimensional array. Each row represents preference information. Each column will contain in and out information.
|  | Please note that caller should create two dimensional array with 2 columns otherwise API fails with invalid argument. The caller should provide preference names in first column only. | 
Option Explicit Sub Example() Dim objApplication As SolidEdgeFramework.Application Dim objTCE As SolidEdgeFramework.SolidEdgeTCE Dim PreferenceInfo(1, 1) As Object Dim PreferenceValue As Object Set objApplication = GetObject(, "SolidEdge.Application") Set objTCE = objApplication.SolidEdgeTCE 'Example takes two preference names PreferenceInfo(0, 0) = "TC_Allow_Longer_ID_Name" PreferenceInfo(1, 0) = "SEEC_BOM_Synchronize" Call objTCE.GetSEECOrTCPreferenceValues(PreferenceInfo) 'Boolean value true or false for preference TC_Allow_Longer_ID_Name PreferenceValue = PreferenceInfo(0, 1) 'Boolean value true or false for preference SEEC_BOM_Synchronize PreferenceValue = PreferenceInfo(1, 1) If Not objApplication Is Nothing Then Call objApplication.Quit End If Set objTCE = Nothing Set objApplication = Nothing End Sub