| Solid Edge Framework Type Library > SolidEdgeTCE Object : IsTeamCenterFileCheckedOut Method |
| Visual Basic |
|---|
Public Function IsTeamCenterFileCheckedOut( _ ByVal bstrFilename As String _ ) As Integer |
This API returns an integer value specifying whether the file is checked out to current user or another user or not checked out to any user.
0 - Not checked out.
1 - Checked out to current user.
2 - Checked out to other user.
Option Explicit Sub Example() Dim objApplication As SolidEdgeFramework.Application Dim objTCE As SolidEdgeFramework.SolidEdgeTCE Dim FileName As String Dim iCheckedOut As Integer Set objApplication = GetObject(, "SolidEdge.Application") Set objTCE = objApplication.SolidEdgeTCE FileName = "F:\009431.par" iCheckedOut = objTCE.IsTeamCenterFileCheckedOut(FileName) If Not objApplication Is Nothing Then Call objApplication.Quit End If Set objTCE = Nothing Set objApplication = Nothing End Sub