| Solid Edge Framework Type Library > SolidEdgeTCE Object : SetTeamCenterMode Method |
| Visual Basic |
|---|
Public Sub SetTeamCenterMode( _ ByVal bMode As Boolean _ ) |
Option Explicit Sub Example() Dim objApplication As SolidEdgeFramework.Application Dim objTCE As SolidEdgeFramework.SolidEdgeTCE Dim bMode As Boolean Set objApplication = GetObject(, "SolidEdge.Application") Set objTCE = objApplication.SolidEdgeTCE bMode = True Call objTCE.SetTeamCenterMode(bMode) If Not objApplication Is Nothing Then Call objApplication.Quit End If Set objTCE = Nothing Set objApplication = Nothing End Sub