Solid Edge Framework Type Library
TextStyle Object Members
Overview 
Public Methods
Public Method GetLineLeadingReturns the line leading and type for the referenced TextStyle object.
Public Method SetLineLeadingSets the line leading and type for the referenced TextStyle object.
Public Properties
Public Property AfterSpacingSets and returns the amount of space below the last line of the paragraph for the referenced text object.
Public Property AlignmentSets and returns the type of text alignment for the referenced TextStyle object.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property BeforeSpacingSets and returns the amount of space above the first line of the paragraph for the referenced text object.
Public Property CharStyleNameSets and returns the character style of the referenced TextStyle object.
Public Property DescriptionReturns a user-specified description of the referenced object.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property LineSpacingGets/Sets the Line spacing of the text style.
Public Property NameReturns the name of the referenced object.
Public Property NumberJustificationSets and returns the number justification for the referenced TextStyle object.
Public Property ParentReturns the parent object for the referenced object.
Public Property UnitsSets and returns the units in which the line width is defined.
See Also

TextStyle Object

Send comments on this topic.