Private Sub Form_Load()
Dim objApp As SolidEdgeframework.Application
Dim objDoc As SolidEdgepart.PartDocument
Dim objVars As SolidEdgeframework.Variables
Dim objVar1 As SolidEdgeframework.variable
Dim objVar2 As SolidEdgeframework.variable
Dim objVarList As SolidEdgeframework.VariableList
Dim strVar1 As String
Dim strFormula1 As String
Dim strVar2 As String
Dim strFormula2 As String
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
' Open the TestCase file
Set objDoc = objApp.Documents.Open(Filename:="T:\vbtests\TestCases\Variables.par")
' Add a new Variable to the already existing Variables
Set objVars = objDoc.Variables
' Set the Variable name and Formula
strVar1 = "MyVar1"
strFormula1 = "2*Height"
Set objVar1 = objVars.Add(pName:=strVar1, pFormula:=strFormula1, UnitsType:=igUnitDistance)
' Query for the existing User created Variables
Set objVarList = objVars.Query(pFindCriterium:="MyVar1")
' Add a new Variable
' Set the Variable name and Formula
strVar2 = "MyVar2"
strFormula2 = "4*Height"
Set objVar2 = objVars.Add(pName:=strVar2, pFormula:=strFormula2, UnitsType:=igUnitDistance)
' Add another Variable to the List
Call objVarList.Add(variable:=objVar2)
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objVars = Nothing
Set objVar1 = Nothing
Set objVar2 = Nothing
Set objVarList = Nothing
End Sub