Private Sub Form_Load()
Dim objApp As SolidEdgeframework.Application
Dim objDoc As SolidEdgepart.PartDocument
Dim objVariables As SolidEdgeframework.Variables
Dim objVariable As SolidEdgeframework.variable
Dim objVar1 As SolidEdgeframework.variable
Dim objVar2 As SolidEdgeframework.variable
Dim lngCount As Long
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'Get Variables Collection
Set objVariables = objDoc.Variables
'Create a variable with Add method
Set objVariable = objVariables.Add(pName:="Variable1", pFormula:="100.0")
'Create a variable specifying UnitType
Set objVar1 = objVariables.Add(pName:="Variable2", pFormula:="100 mm", UnitsType:=igUnitDistance)
'Create a variable with Formula
Set objVar2 = objVariables.Add(pName:="Variable3", pFormula:="Variable1 * Variable2", UnitsType:=igUnitArea)
'Get the count of variables created
lngCount = objVariables.Count
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objVariables = Nothing
Set objVariable = Nothing
Set objVar1 = Nothing
Set objVar2 = Nothing
End Sub