Private Sub Form_Load()
Dim objApp As SolidEdgeframework.Application
Dim objDoc As SolidEdgepart.PartDocument
Dim objVariables As SolidEdgeframework.Variables
Dim objVariable As SolidEdgeframework.variable
Dim objVar1 As SolidEdgeframework.variable
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'Get Variables Collection
Set objVariables = objDoc.Variables
'Create a variable with Add method
Set objVariable = objVariables.Add(pName:="Variable1", pFormula:="100.0")
'Get the Variable object with Translate method
Set objVar1 = objVariables.Translate(pName:="Variable1")
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objVariables = Nothing
Set objVariable = Nothing
Set objVar1 = Nothing
End Sub