|  AddLight | Adds a light to the referenced ViewStyle object. | 
|  BeginPropertyBuffer |  | 
|  Delete | Deletes the referenced object. | 
|  DeleteLight | Deletes a light from the referenced ViewStyle object. | 
|  FlushPropertyBuffer | Flushes the property buffer for the referenced FaceStyle or ViewStyle object. | 
|  GetAnalysisParameters | Returns the analysis parameters of the referenced ViewStyle object. | 
|  GetGradientBackground |  | 
|  GetGradientColor |  | 
|  GetLight | Returns the parameters of a specified light for the referenced ViewStyle object. | 
|  GetLightColor | Returns the color of a specified light for the referenced ViewStyle object. | 
|  GetLightIntensity | Returns the intensity of a specified light for the referenced ViewStyle object. | 
|  GetLightPhi | Returns the angle of the rotation in a spherical coordinate system of a specified light relative to the target for the referenced ViewStyle object. | 
|  GetLightTheta | Returns the angle of the sweep in a spherical coordinate system of a specified light relative to the target for the referenced ViewStyle object. | 
|  GetSkyboxOrientation | Returns the orientation of the skybox used in the referenced ViewStyle object. | 
|  GetSkyboxSideFilename | Returns the file name of the image used on one side of the skybox in the referenced ViewStyle object. | 
|  SetAnalysisParameters | Sets the analysis parameters of the referenced ViewStyle object. | 
|  SetGradientBackground |  | 
|  SetGradientColor |  | 
|  SetLight | Sets the parameters of a specified light for the referenced ViewStyle object. | 
|  SetLightColor | Sets the color of a specified light for the referenced ViewStyle object. | 
|  SetLightIntensity | Sets the intensity of a specified light for the referenced ViewStyle object. | 
|  SetLightPhi | Sets the angle of the rotation in a spherical coordinate system of a specified light relative to the target for the referenced ViewStyle object. | 
|  SetLightTheta | Sets the angle of the sweep in a spherical coordinate system of a specified light relative to the target for the referenced ViewStyle object. | 
|  SetSkyboxOrientation | Sets the orientation of the skybox used in the referenced ViewStyle object. | 
|  SetSkyboxSideFilename | Sets the file name of the image used on one side of the skybox in the referenced ViewStyle object. | 
|  SetSkyboxSkyFile | Sets the name of the sky file used to define the skybox in the referenced ViewStyle object. | 
|  SkyboxClear | Clears the image from one side of the skybox in the referenced ViewStyle object. | 
|  SkyboxClearAll | Clears the images from all sides of the skybox in the referenced ViewStyle object. |