Solid Edge Framework Type Library
Expose Property
Collapse All
Expand All
Solid Edge Framework Type Library
>
variable Object
: Expose Property
Description
This read-write Long property sets and returns whether the referenced object is exposed as a custom property. When set to 1, the object is exposed; when set to 0, the object is not exposed.
Property type
Read-write property
Syntax
Visual Basic
Public Property Expose As Long
See Also
variable Object
|
variable Members
Send comments
on this topic.